© 2007 Cummins Inc.



Links Buy Online Home
Downloads:
QC Configurator
 

QC Configurator Software Download

The QC Configurator installation is a typical Windows-based, self-executing installation. Note that you only need to install the QC Configurator program separately if you are using QuickCheck II instead of QuickCheck III (QC Configurator is already part of the QuickCheck III installation). The install program sets up the application for the handheld organizer.

The steps for the QC Configurator software installation are listed below. It is already assumed that you have previously installed the handheld Desktop software. If you have not installed this software, see the handheld handbook for instructions on installing the Desktop software.

  1. Download the QC Configurator zip file by clicking on the button above.
  2. Unzip the executable file using zip/unzip software.
  3. Click on the Windows Start menu and click Run.
  4. Click on the Browse button and locate the file you have downloaded.
  5. Click the OK button to install the QC Configurator program.
  6. Follow the onscreen instructions to complete the installation. The installation places all PC components into the root directory of the handheld organizer (typically C:\Palm or C:\Program Files\Palm). However, QC Configurator components are placed in the \qc2 (or \qc3 if you have QuickCheck III) directory immediately below the Palm root directory.
  7. Perform a HotSync operation to install the QC Configurator application on the handheld organizer.


In case of difficulties, please consult the QC Configurator for QuickCheck II User's Manual.