The QuickSpec installation
is a typical Windows-based, self-executing installation. It sets up
the application for the handheld organizer and also installs
the
QuickSpec Conduit,
which is used by the HotSync Manager to send the stored engine data from
the handheld organizer to the host PC. You must have a QuickCheck III adapter
for the QuickSpec application to work.
The steps for the QuickSpec
software installation are listed below. It is already assumed
that
you have previously installed the handheld Desktop software. If you have
not installed this
software, see the handheld handbook for instructions on installing the
Desktop software.
Download the QuickSpec zip file
by clicking on the button above.
Unzip the executable file using zip/unzip software.
Click on the Windows
Start menu and click Run.
Click on the Browse button and locate the file you have downloaded.
Click the OK button
to install the QuickSpec desktop component (the Conduit), which
will also register the Palm Application with the
Palm HotSync Manager.
Follow the onscreen
instructions to complete the installation. The installation places
all PC
components into the root directory of the handheld organizer
(typically C:\Palm or C:\Program Files\Palm).
However, QuickTrip components are placed in the \qSpec directory
immediately below the Palm root directory.
Perform a HotSync
operation to install the QuickSpec application on the handheld
organizer.