© 2007 Cummins Inc.



Links Buy Online Home
Downloads:
QuickTrip
 

QuickTrip Software Download

The QuickTrip installation is a typical Windows-based, self-executing installation. It sets up the application for the handheld organizer and also installs the QuickTrip Conduit, which is used by the HotSync Manager to send the stored engine data from the handheld organizer to the host PC. You must have a QuickCheck III adapter for the QuickTrip application to work.

The steps for the QuickTrip software installation are listed below. It is already assumed that you have previously installed the handheld Desktop software. If you have not installed this software, see the handheld handbook for instructions on installing the Desktop software.

  1. Download the QuickTrip zip file by clicking on the button above.
  2. Unzip the executable file using zip/unzip software.
  3. Click on the Windows Start menu and click Run.
  4. Click on the Browse button and locate the file you have downloaded.
  5. Click the OK button to install the QuickTrip desktop component (the Conduit), which will also register the Palm Application with the Palm HotSync Manager.
  6. Follow the onscreen instructions to complete the installation. The installation places all PC components into the root directory of the handheld organizer (typically C:\Palm or C:\Program Files\Palm). However, QuickTrip components are placed in the \qTrip directory immediately below the Palm root directory.
  7. Perform a HotSync operation to install the QuickTrip application on the handheld organizer.


In case of difficulties, please consult the QuickTrip User's Manual.