Links Buy Online Home
FAQ:
 
 
 

Before requesting support, please experiment a bit to reproduce and isolate the problem. When you do contact support, please be ready to provide the following information:

  • The version of the Windows operating system you are using on your PC
  • The actual error message or state that you are experiencing
  • The steps you take to reproduce the problem
  • The version of Windows® CE software you are using and available memory
  • The version of PowerSpec CE, QuickCheck CE, or other application software you are using
  • The version of ActiveSync® Manager you are using on your PC

To find Windows® operating system version information:

  1. Click the Start menu in the Windows® system tray on the bottom left side of your computer screen in the Taskbar.
  2. Choose Settings, then click Control Panel.
  3. Double-Click System.

To find Windows® CE version and memory information:

  1. Tap the Start menu icon in the lower left corner of the QC5100.
  2. Tap Settings, then Control Panel.
  3. Scroll down and Double-tap System.
  4. Tap Versions tab to see version numbers, and tap Memory tab to see the amount of storage and program memory, in kiloBytes (KB).

To find PowerSpec CE, QuickCheck CE, or other application version information:

  1. Tap the application icon.
  2. Tap the Help (or Options) Menu in the application.
  3. Tap About.

To find ActiveSync® Manager version information:

  1. Click the ActiveSync® Manager icon in the Windows system tray on the bottom right side of your computer screen in the Taskbar.
  2. Click Open Microsoft Active Sync.
  3. Click Help, then About.

 

Click on a Frequently Asked Questions link at upper left to reach the page that addresses that particular topic.

 

© 2009 Cummins Inc.