Microsoft Internet Explorer
version 5.01 or higher
Please Note: QuickReport 4.0 requires Microsoft .NET Framework Version 2.0. For convenience, the update to .NET 2.0 can be downloaded by clicking on the following link: .NET 2.0 Framework. After downloading, just unzip and run the self-executable file.
QuickReport product consists
of:
QuickReport software CD (P/N
3165172)
QuickReport Windows:
QuickReport Graphical User Interface Window
Displays start and stop dates for the desired time period of the vehicle usage report
Provides vehicle list to select from for the report, including options to select or deselect all vehicles
Shows trip parameter selections to include in report, with a maximum limit of seven selections
Can display a quick history of items selected in desired units
QuickHistory Window
Displays the extraction information on the vehicle, time period, and data for parameter list selected in the QuickReport Graphical User Interface window
Allows sorting of the data by clicking the column title of the column you want to base the sorting on, with subsequent clicks changing the sort format from descending to ascending order
Extraction Detail Report Print Preview Window
Shows the actual print format of the report for a particular vehicle after right-clicking on a row in the QuickHistory window
If the report looks OK, you can print the report or close without printing
History Report Print Preview Window
Shows the actual print format of the report after clicking the Print Preview button in the QuickHistory window
If the report looks OK, you can print the report or close without printing